This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: Modifying refresh rate of the projector of the DLP4500

Part Number: DLP4500
Other Parts Discussed in Thread: DLPC350

Hello,

I've heard that the default refresh rate of the DLP4500 is 120Hz. Suppose I connect it to a 60Hz display and project it out, I am assuming that the refresh of the project image still happens at 120Hz. How do I modify the refresh rate of the projector to make it work at 60Hz