Other Parts Discussed in Thread: DLP4500
Hi there,
I have defined a pattern sequence into the LUT. When displaying the pattern, I would like to pause the pattern in between for a few seconds, and then continue the pattern sequence. But I have two issues regarding this process:
1. While pausing, the projector immediately give a dark scene. However, I would like the current pattern to hold still. Is it possible to achieve this function?
- I am guessing that the LED goes off automatically when paused, but I have no idea how to get around this.
2. When I resume the pattern sequence, I have to wait for the current pattern to finish up its remaining exposure time before jumping to the next pattern. Is it possible to skip the current pattern and jump to the next one?
- According to the DLPC350 Programmer Guide, TRIG_OUT_2 indicates the start of a pattern. I am wondering if I can manually set it to 1 so that I can force the next pattern to show up. The only section I found related to TRIG_OUT_2 is section 2.4.3.2.3. However, this control requires stopping and re-validating of the pattern sequence. Re-validation means LED must be off and thus doesn't fit my need in issue 1.
FYI, I am using Pattern Sequence Mode with pattern from flash memory, using Trigger Mode 1.
Thank you,
Jeff Leung