This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DLPC3433: Configure DLPC3433 (external video source with RGB565 input) in IMX6

Part Number: DLPC3433

Tool/software: Linux

Hi,

I need to configure the DLPC3433 (mipi_DSI)  in the IMX6 board. I couldn't find any driver for DLPC3433.

Can you help me to configure DLPC3433  in the IMX6 with external video source RGB565 input.

Thanks in Advance

Anurag Raghavan.

  • Hello Anurag,

    Is this the board you are referring to: boundarydevices.com/.../ If it is, it looks like it has a 24-bit RGB interface which could be used for RGB888 input. If their board supports it, perhaps it could also input RGB565. However, it doesn't look like it has a DSI interface.

    The DLPC3433 is designed to accept any video input that meets its required specifications. It may need to be configured via I2C for the appropriate input; however, it doesn't have other device specific drivers for video.

    Thanks,
    Kyle
  • Hello Anurag,

    Please let me know if you still need assistance. I will be closing this thread for now.

    Thanks,
    Kyle