This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/DLPC2607: dlpc2607, dmd2000

Part Number: DLPC2607

Tool/software: TI C/C++ Compiler

HI...

I am using DMD2000 and DLPC2607 for my post graduation project. [I am not using Lightcrafter EVM]

I want to know that does DLPC2607 needs to be programmed?

Thanks and regards,

Trupti

  • Trupti,

    The DLPC2607 has a standard firmware release. You cannot modify this firmware outside of requesting revised firmware with custom looks/duty cycle configurations. What are you trying to do with the DLPC2607?

    Best Regards,
    Philippe Dollo
  • Sir,
    I want make prototype for wearable glasses as a part of my post graduation project. So I just wanted to confirm few things before.
    As I am not using light crafter EVM, I am using it's design files for altered version.
    So, thing is I just have to program or write software for my host processor (I am using Raspberry Pi ), and DLPC will be provided with it's firmware. Is it correct?
  • Trupti,

    That is partially correct. For the firmware, you can either grab it off of the flash on the EVM itself or request a flash image from us via private message. The firmware is already created, but you will need to write the image to a part yourself.

    I hope this helps.

    Best Regards,
    Philippe Dollo