This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR4500EVM: Problems flashing with Lightcrafter software

Part Number: DLPLCR4500EVM

Team,

my customer is using the Lightcrafter 4500 Modules. They have issues with flashing the device using the Lightcrafter Software. Sometimes it works, sometimes it does not work. In case it does not work, they get error message "Flash Manufacturer ID" error.

The modules are not modified (HW and SW).
They are using Lightcrafter software 3.0.1 and 3.1.0. Sometimes one of them works, sometimes the other version works. sometimes non of them does.

Do you have a method to reliably flash the devices?

Thanks!

  • Hello,

    Do you know what version of firmware the customer has installed on the Lightcrafter4500? The DLP LightCrafter 4500 EVM GUI is the generally recommended way to flash the EVM.

    Thanks,
    Kyle
  • Hi Kyle,

    The Lightcrafter modules have different firmware versions. Some have original TI firmware (v3.1 or v4.0), some modules have their custom firmware on them.
    The bootloader is always untouched though.

    Have you encountered this before?
    Do you think the operating system may be factor for this?

    Thanks
  • Kyle,
    do you have feedback for me?
    Thanks
  • btw, they are using Windows 10 and have tested this on various PCs.
  • Any feedback would be highly appreciated.
  • Hi Franziskus,

    Do you have the same problem in BOOT_HOLD mode also? Could you kindly try shorting J18 and then try to upload the code and see if you face the same issue? This information will really help us debug the issue. Could you also kindly confirm the model of the flash chip that is on your LCR4500?

    Thanks & Regards,
    Hirak.
  • Hello Hirak,

    thanks for the advice. In order not to molest Fanziskus too much I will reply directly.

    We tested flashing in Boot-hold mode but the result was the same. The flash which is solderd is a Spansion S29GL064A.

    We can flash via JTAG, however for production this would be to slow.

    Thanks

    Richard

  • Hi Richard,

    Kindly try this: locate the file "FlashDeviceParameters.txt" in the installation directory of LCR4500 GUI, and replace the file with the one that is attached herewith and then try flashing again. 

    Hope this helps,

    Thanks & Regards,

    Hirak.

    // Flash Device Information.
    // DDP1000 & DDP1010
    // 03/07/2001
    // 03/22/2002 Added AT49B(L)V8192A and fixed sector addresses for AT49BV4096A - crb
    // 09/12/2006 Added Spansion S29GL032A - rah
    //
    // Mfg      MfgID           Device   DevID   Mb Alg     Size #sec  Sector_Addresses
    "AMD",      0x0001,    "Am29LV400B", 0x22BA,  4, 0,  0x80000, 11,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "AMD",      0x0001,    "Am29LV800B", 0x225B,  8, 0, 0x100000, 19,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "AMD",      0x0001,    "Am29DL800B", 0x22CB,  8, 0, 0x100000, 19,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "AMD",      0x0001,    "Am29LV160D", 0x2249, 16, 0, 0x200000, 35,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0, 0, 0, 0, 0, 
    "Fujitsu",  0x0004,  "MBM29LV400BC", 0x22BA,  4, 0,  0x80000, 11,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Fujitsu",  0x0004,  "MBM29LV800BA", 0x225B,  8, 0, 0x100000, 19,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Fujitsu",  0x0004,  "MBM29LV160BE", 0x2249, 16, 0, 0x200000, 35,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0, 0, 0, 0, 0, 
    "Hyundai",  0x00AD,     "HY29LV160", 0x2249, 16, 0, 0x200000, 35,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0, 0, 0, 0, 0, 
    "Intel",    0x0089,      "28F400B3", 0x8895,  4, 1,  0x80000, 15,  0, 0x2000, 0x4000, 0x6000, 0x8000,  0xA000,  0xC000,  0xE000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0,	0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Intel",    0x0089,      "28F800B3", 0x8893,  8, 1, 0x100000, 23,  0, 0x2000, 0x4000, 0x6000, 0x8000,  0xA000,  0xC000,  0xE000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000,  0xD0000,  0xE0000,  0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Intel",    0x0089,      "28F160B3", 0x8891, 16, 1, 0x200000, 39,  0, 0x2000, 0x4000, 0x6000, 0x8000,  0xA000,  0xC000,  0xE000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000,  0xD0000,  0xE0000,  0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0,
    "Intel",    0x0089,      "28F320B3", 0x8897, 32, 1, 0x400000, 71,  0, 0x2000, 0x4000, 0x6000, 0x8000,  0xA000,  0xC000,  0xE000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000,  0xD0000,  0xE0000,  0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0x210000, 0x220000, 0x230000, 0x240000, 0x250000, 0x260000, 0x270000, 0x280000, 0x290000, 0x2A0000, 0x2B0000, 0x2C0000, 0x2D0000, 0x2E0000, 0x2F0000, 0x300000, 0x310000, 0x320000, 0x330000, 0x340000, 0x350000, 0x360000, 0x370000, 0x380000, 0x390000, 0x3A0000, 0x3B0000, 0x3C0000, 0x3D0000, 0x3E0000, 0x3F0000,
    "Intel",    0x0089,      "28F800C3", 0x88C1,  8, 1, 0x100000, 23,  0, 0x2000, 0x4000, 0x6000, 0x8000,  0xA000,  0xC000,  0xE000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000,  0xD0000,  0xE0000,  0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Intel",    0x0089,      "28F160C3", 0x88C3, 16, 1, 0x200000, 39,  0, 0x2000, 0x4000, 0x6000, 0x8000,  0xA000,  0xC000,  0xE000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000,  0xD0000,  0xE0000,  0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0,
    "Macronix", 0x00C2,    "MX29LV800B", 0x225B,  8, 0, 0x100000, 19,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Spansion", 0x0001,     "S29GL032A", 0x227E, 32, 0, 0x400000, 71,  0, 0x2000, 0x4000, 0x6000, 0x8000,  0xA000,  0xC000,  0xE000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000,  0xD0000,  0xE0000,  0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0x210000, 0x220000, 0x230000, 0x240000, 0x250000, 0x260000, 0x270000, 0x280000, 0x290000, 0x2A0000, 0x2B0000, 0x2C0000, 0x2D0000, 0x2E0000, 0x2F0000, 0x300000, 0x310000, 0x320000, 0x330000, 0x340000, 0x350000, 0x360000, 0x370000, 0x380000, 0x390000, 0x3A0000, 0x3B0000, 0x3C0000, 0x3D0000, 0x3E0000, 0x3F0000,
    "STM",      0x0020,     "M29W400BB", 0x00EF,  4, 0,  0x80000, 11,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "STM",      0x0020,     "M29W800AB", 0x005B,  8, 0, 0x100000, 19,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "STM",      0x0020,     "M29W160BB", 0x2249, 16, 0, 0x200000, 35,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0, 0, 0, 0, 0, 
    "STM",      0x0020,     "M29W800DB", 0x225B,  8, 0, 0x100000, 19,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "STM",      0x0020,     "M29W128GL", 0x227E, 256, 0, 0x4000000, 256,  0x000000,0x020000,0x040000,0x060000,0x080000,0x0A0000,0x0C0000,0x0E0000,0x100000,0x120000,0x140000,0x160000,0x180000,0x1A0000,0x1C0000,0x1E0000,0x200000,0x220000,0x240000,0x260000,0x280000,0x2A0000,0x2C0000,0x2E0000,0x300000,0x320000,0x340000,0x360000,0x380000,0x3A0000,0x3C0000,0x3E0000,0x400000,0x420000,0x440000,0x460000,0x480000,0x4A0000,0x4C0000,0x4E0000,0x500000,0x520000,0x540000,0x560000,0x580000,0x5A0000,0x5C0000,0x5E0000,0x600000,0x620000,0x640000,0x660000,0x680000,0x6A0000,0x6C0000,0x6E0000,0x700000,0x720000,0x740000,0x760000,0x780000,0x7A0000,0x7C0000,0x7E0000,0x800000,0x820000,0x840000,0x860000,0x880000,0x8A0000,0x8C0000,0x8E0000,0x900000,0x920000,0x940000,0x960000,0x980000,0x9A0000,0x9C0000,0x9E0000,0xA00000,0xA20000,0xA40000,0xA60000,0xA80000,0xAA0000,0xAC0000,0xAE0000,0xB00000,0xB20000,0xB40000,0xB60000,0xB80000,0xBA0000,0xBC0000,0xBE0000,0xC00000,0xC20000,0xC40000,0xC60000,0xC80000,0xCA0000,0xCC0000,0xCE0000,0xD00000,0xD20000,0xD40000,0xD60000,0xD80000,0xDA0000,0xDC0000,0xDE0000,0xE00000,0xE20000,0xE40000,0xE60000,0xE80000,0xEA0000,0xEC0000,0xEE0000,0xF00000,0xF20000,0xF40000,0xF60000,0xF80000,0xFA0000,0xFC0000,0xFE0000,0x1000000,0x1020000,0x1040000,0x1060000,0x1080000,0x10A0000,0x10C0000,0x10E0000,0x1100000,0x1120000,0x1140000,0x1160000,0x1180000,0x11A0000,0x11C0000,0x11E0000,0x1200000,0x1220000,0x1240000,0x1260000,0x1280000,0x12A0000,0x12C0000,0x12E0000,0x1300000,0x1320000,0x1340000,0x1360000,0x1380000,0x13A0000,0x13C0000,0x13E0000,0x1400000,0x1420000,0x1440000,0x1460000,0x1480000,0x14A0000,0x14C0000,0x14E0000,0x1500000,0x1520000,0x1540000,0x1560000,0x1580000,0x15A0000,0x15C0000,0x15E0000,0x1600000,0x1620000,0x1640000,0x1660000,0x1680000,0x16A0000,0x16C0000,0x16E0000,0x1700000,0x1720000,0x1740000,0x1760000,0x1780000,0x17A0000,0x17C0000,0x17E0000,0x1800000,0x1820000,0x1840000,0x1860000,0x1880000,0x18A0000,0x18C0000,0x18E0000,0x1900000,0x1920000,0x1940000,0x1960000,0x1980000,0x19A0000,0x19C0000,0x19E0000,0x1A00000,0x1A20000,0x1A40000,0x1A60000,0x1A80000,0x1AA0000,0x1AC0000,0x1AE0000,0x1B00000,0x1B20000,0x1B40000,0x1B60000,0x1B80000,0x1BA0000,0x1BC0000,0x1BE0000,0x1C00000,0x1C20000,0x1C40000,0x1C60000,0x1C80000,0x1CA0000,0x1CC0000,0x1CE0000,0x1D00000,0x1D20000,0x1D40000,0x1D60000,0x1D80000,0x1DA0000,0x1DC0000,0x1DE0000,0x1E00000,0x1E20000,0x1E40000,0x1E60000,0x1E80000,0x1EA0000,0x1EC0000,0x1EE0000,0x1F00000,0x1F20000,0x1F40000,0x1F60000,0x1F80000,0x1FA0000,0x1FC0000,0x1FE0000, 0x2000000, 0x204000, 0x2060000,0x2080000,0x20A0000,0x20C0000,0x20E0000,0x2100000,0x2120000,0x2140000,0x2160000,0x2180000,0x21A0000,0x21C0000,0x21E0000,0x2200000,0x2220000,0x2240000,0x2260000,0x2280000,0x22A0000,0x22C0000,0x22E0000,0x2300000,0x2320000,0x2340000,0x2360000,0x2380000,0x23A0000,0x23C0000,0x23E0000,0x2400000,0x2420000,0x2440000,0x2460000,0x2480000,0x24A0000,0x24C0000,0x24E0000,0x2500000,0x2520000,0x2540000,0x2560000,0x2580000,0x25A0000,0x25C0000,0x25E0000,0x2600000,0x2620000,0x2640000,0x2660000,0x2680000,0x26A0000,0x26C0000,0x26E0000,0x2700000,0x2720000,0x2740000,0x2760000,0x2780000,0x27A0000,0x27C0000,0x27E0000,0x2800000,0x2820000,0x2840000,0x2860000,0x2880000,0x28A0000,0x28C0000,0x28E0000,0x2900000,0x2920000,0x2940000,0x2960000,0x2980000,0x29A0000,0x29C0000,0x29E0000,0x2A00000,0x2A20000,0x2A40000,0x2A60000,0x2A80000,0x2AA0000,0x2AC0000,0x2AE0000,0x2B00000,0x2B20000,0x2B40000,0x2B60000,0x2B80000,0x2BA0000,0x2BC0000,0x2BE0000,0x2C00000,0x2C20000,0x2C40000,0x2C60000,0x2C80000,0x2CA0000,0x2CC0000,0x2CE0000,0x2D00000,0x2D20000,0x2D40000,0x2D60000,0x2D80000,0x2DA0000,0x2DC0000,0x2DE0000,0x2E00000,0x2E20000,0x2E40000,0x2E60000,0x2E80000,0x2EA0000,0x2EC0000,0x2EE0000,0x2F00000,0x2F20000,0x2F40000,0x2F60000,0x2F80000,0x2FA0000,0x2FC0000,0x2FE0000, 0x3000000, 0x3020000,0x3040000,0x3060000,0x3080000,0x30A0000,0x30C0000,0x30E0000,0x3100000,0x3120000,0x3140000,0x3160000,0x3180000,0x31A0000,0x31C0000,0x31E0000,0x3200000,0x3220000,0x3240000,0x3260000,0x3280000,0x32A0000,0x32C0000,0x32E0000,0x3300000,0x3320000,0x3340000,0x3360000,0x3380000,0x33A0000,0x33C0000,0x33E0000,0x3400000,0x3420000,0x3440000,0x3460000,0x3480000,0x34A0000,0x34C0000,0x34E0000,0x3500000,0x3520000,0x3540000,0x3560000,0x3580000,0x35A0000,0x35C0000,0x35E0000,0x3600000,0x3620000,0x3640000,0x3660000,0x3680000,0x36A0000,0x36C0000,0x36E0000,0x3700000,0x3720000,0x3740000,0x3760000,0x3780000,0x37A0000,0x37C0000,0x37E0000,0x3800000,0x3820000,0x3840000,0x3860000,0x3880000,0x38A0000,0x38C0000,0x38E0000,0x3900000,0x3920000,0x3940000,0x3960000,0x3980000,0x39A0000,0x39C0000,0x39E0000,0x3A00000,0x3A20000,0x3A40000,0x3A60000,0x3A80000,0x3AA0000,0x3AC0000,0x3AE0000,0x3B00000,0x3B20000,0x3B40000,0x3B60000,0x3B80000,0x3BA0000,0x3BC0000,0x3BE0000,0x3C00000,0x3C20000,0x3C40000,0x3C60000,0x3C80000,0x3CA0000,0x3CC0000,0x3CE0000,0x3D00000,0x3D20000,0x3D40000,0x3D60000,0x3D80000,0x3DA0000,0x3DC0000,0x3DE0000,0x3E00000,0x3E20000,0x3E40000,0x3E60000,0x3E80000,0x3EA0000,0x3EC0000,0x3EE0000,0x3F00000,0x3F20000,0x3F40000,0x3F60000,0x3F80000,0x3FA0000,0x3FC0000,0x3FE0000, 
    "Toshiba",  0x0098,    "TC58FVB400", 0x004C,  4, 2,  0x80000, 11,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Toshiba",  0x0098,    "TC58FVB800", 0x00CE,  8, 2, 0x100000, 19,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Toshiba",  0x0098,  "TC58FVB160FT", 0x0043, 16, 0, 0x200000, 35,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0, 0, 0, 0, 0, 
    "Toshiba",  0x0098,  "TC58FYB160FT", 0x0023, 16, 0, 0x200000, 35,  0,         0x4000, 0x6000, 0x8000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0, 0, 0, 0, 0, 
    "Micron",   0x0089,    "MT28F400B3", 0x4471,  4, 1,  0x80000,  7,  0,         0x4000, 0x6000, 0x8000, 0x20000, 0x40000, 0x60000, 0x80000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Micron",   0x0089,    "MT28F800B3", 0x889D,  8, 1, 0x100000, 11,  0,         0x4000, 0x6000, 0x8000, 0x20000, 0x40000, 0x60000, 0x80000, 0xA0000, 0xC0000, 0xE0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0,
    "Micron",   0x002C,    "MT28F160A3", 0x4491, 16, 1, 0x200000, 40,  0, 0x2000, 0x4000, 0x6000, 0x8000, 0xA000,  0xC000,  0xE000,  0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000,  0xD0000,  0xE0000,  0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000,
    "Sharp",    0x00B0,   "LH28F400BVE", 0x005A,  4, 1,  0x80000, 15,  0, 0x2000, 0x4000, 0x6000, 0x8000,  0xA000,  0xC000,  0xE000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0,	0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Sharp",    0x00B0,   "LH28F800BVE", 0x004B,  8, 1, 0x100000, 23,  0, 0x2000, 0x4000, 0x6000, 0x8000,  0xA000,  0xC000,  0xE000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000,  0xD0000,  0xE0000,  0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 
    "Sharp",    0x00B0,  "LH28F160BVHE", 0x0049, 16, 1, 0x200000, 39,  0, 0x2000, 0x4000, 0x6000, 0x8000,  0xA000,  0xC000,  0xE000, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000,  0xD0000,  0xE0000,  0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0,
    "Atmel",    0x161F,   "AT49BV4096A", 0x1692,  4, 2,  0x80000,  4,  0, 0x4000, 0x6000, 0x8000, 0x80000, 0, 0, 0,	0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0,
    "Atmel",    0x001F, "AT49B(L)V8011", 0x00CB,  8, 2, 0x100000, 22,  0,         0x4000, 0xC000, 0xE000, 0x10000, 0x12000, 0x14000, 0x1C000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0,
    "Atmel",    0x001F,    "AT49BV1614", 0x00C0, 16, 2, 0x200000, 39,  0, 0x2000, 0x4000, 0x6000, 0x8000, 0xA000,  0xC000,  0xE000, 0x10000, 0x18000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0,
    "Atmel",    0x001F,"AT49B(L)V8192A", 0x00A0,  8, 2, 0x100000,  4,  0, 0x4000, 0x6000, 0x8000, 0x100000,0, 0, 0,   0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0
    //
    // DDP3020 Serial Flash Parts (serial parts have "Alg" values >= 10)
    //
    // Mfg      MfgID           Device   DevID   Mb Alg     Size #sec  Sector_Addresses                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                         PageSize (optional)
    "STM",      0x0020,        "M25P32", 0x2016, 32,10, 0x400000, 64,  0, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, 0x90000, 0xA0000, 0xB0000, 0xC0000, 0xD0000, 0xE0000, 0xF0000, 0x100000, 0x110000, 0x120000, 0x130000, 0x140000, 0x150000, 0x160000, 0x170000, 0x180000, 0x190000, 0x1A0000, 0x1B0000, 0x1C0000, 0x1D0000, 0x1E0000, 0x1F0000, 0x200000, 0x210000, 0x220000, 0x230000, 0x240000, 0x250000, 0x260000, 0x270000, 0x280000, 0x290000, 0x2A0000, 0x2B0000, 0x2C0000, 0x2D0000, 0x2E0000, 0x2F0000, 0x300000, 0x310000, 0x320000, 0x330000, 0x340000, 0x350000, 0x360000, 0x370000, 0x380000, 0x390000, 0x3A0000, 0x3B0000, 0x3C0000, 0x3D0000, 0x3E0000, 0x3F0000, 256
    //
    // DLPC350 Testing 05182018
    //
    // Mfg      MfgID    Device       DevID   Mb  Alg   Size    #sec  Sector_Addresses                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                         PageSize (optional)
    "Micron",   0x0089, "MT28EW128", 0x227E, 128, 0, 0x1000000, 128, 0x0, 0x20000, 0x40000, 0x60000, 0x80000, 0xA0000, 0xC0000, 0xE0000, 0x100000, 0x120000, 0x140000, 0x160000, 0x180000, 0x1A0000, 0x1C0000, 0x1E0000, 0x200000, 0x220000, 0x240000, 0x260000, 0x280000, 0x2A0000, 0x2C0000, 0x2E0000, 0x300000, 0x320000, 0x340000, 0x360000, 0x380000, 0x3A0000, 0x3C0000, 0x3E0000, 0x400000, 0x420000, 0x440000, 0x460000, 0x480000, 0x4A0000, 0x4C0000, 0x4E0000, 0x500000, 0x520000, 0x540000, 0x560000, 0x580000, 0x5A0000, 0x5C0000, 0x5E0000, 0x600000, 0x620000, 0x640000, 0x660000, 0x680000, 0x6A0000, 0x6C0000, 0x6E0000, 0x700000, 0x720000, 0x740000, 0x760000, 0x780000, 0x7A0000, 0x7C0000, 0x7E0000, 0x800000, 0x820000, 0x840000, 0x860000, 0x880000, 0x8A0000, 0x8C0000, 0x8E0000, 0x900000, 0x920000, 0x940000, 0x960000, 0x980000, 0x9A0000, 0x9C0000, 0x9E0000, 0xA00000, 0xA20000, 0xA40000, 0xA60000, 0xA80000, 0xAA0000, 0xAC0000, 0xAE0000, 0xB00000, 0xB20000, 0xB40000, 0xB60000, 0xB80000, 0xBA0000, 0xBC0000, 0xBE0000, 0xC00000, 0xC20000, 0xC40000, 0xC60000, 0xC80000, 0xCA0000, 0xCC0000, 0xCE0000, 0xD00000, 0xD20000, 0xD40000, 0xD60000, 0xD80000, 0xDA0000, 0xDC0000, 0xDE0000, 0xE00000, 0xE20000, 0xE40000, 0xE60000, 0xE80000, 0xEA0000, 0xEC0000, 0xEE0000, 0xF00000, 0xF20000, 0xF40000, 0xF60000, 0xF80000, 0xFA0000, 0xFC0000, 0xFE0000,
    

  • Hi Hirak,

    thanks so much. This actually worked. Since we have the 64MB Version of the chip we will try adjusting the file so that we can use all sectors. It should only be a matter of changing the Nr of sectors and the sector adresses, right?

    Tanks again

    Richard
  • Hi Richard, yes, kindly confirm and modify the total size, sector number and sector addresses to use your new flash.

    If we were able to solve your issue, kindly mark the answer as "resolved". 


    Thanks & Regards,
    Hirak.