Dear Ti support, Hi !
I have the DLP LightCrafter4500 and I want to use it to trigger my camera DCC3240C: https://www.thorlabs.com/thorproduct.cfm?partnumber=DCC3240C
My DLP trigger output 2 is a - 3.3V signal but the trigger level low of the camera is 0-1V and the trigger level high is 5-24V.
I had the same problem with my previous camera that I could not trigger because of that. It seems that many cameras cannot be triggered using the light output voltage. Am I missing something ? Do you have any advice so I could use my light to trigger my camera ? (I am not familiar with the electrical engineering even if I have the very basics of it)
Thank you very much for you support,
Have a nice day,
Emilie