This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: FPC cable Connection between DLPC3439 and DLP4710

Part Number: DLP4710EVM-LC
Other Parts Discussed in Thread: DLP4710, , DLPC3479

Hello TI Expert,

 

I have got a quesiton about the connection of DLP4710 and two DLPC3439s.

Since my cusomer is considering to make their own DLP prototypes, we would like to check the connection about J22 connector of DLP4710EVM-LC.

Would you please answer the question?

 

[Queston]

There are 2 sets of 4 control pins on the J22 connector.

EXT_M_SPI_CLK, EXT_M_SPI_DOUT, EXT_M_SPI_DIN, EXT_M_SPI_CSZ (32-35pin)

EXT_S_SPI_CLK, EXT_S_SPI_DOUT, EXT_S_SPI_DIN, EXT_S_SPI_CSZ (76-80pin)

 

Would you please tell us what is the purpose of these signals?

If these signals are not needed for them, they want to remove these signals to reduce pins.

 

Please tell us whether these signals are needed or not.

 

 

Thank you for your commnet.

 

Nobu Arai