Due to the U.S. Thanksgiving holiday, please expect delayed responses during the week of 11/22.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP5531Q1EVM: DLP5531-Q1 EVM Formatter Board Faulty

Part Number: DLP5531Q1EVM
Other Parts Discussed in Thread: DLP5531-Q1

Hello,

I have an evaluation board from you, DLP5531Q1EVM, and when I try to display an image, on the DMD, image is wrong, only half is displayed. Also in GUI I have an error: DMD Training Error.

Also, i put another DLP5531-Q1 EVM Formatter Board with the same DMD and image was OK. It looks like a faulty DLP5531-Q1 EVM Formatter Board.

What is your opinion?

Thank you,

Marian.