I'm finding that the documentation is not really clear regarding calibration/correction of data. Take for example the reflectance values. Are the values internally corrected due to a factory calibration and therefore the raw values transferred to my excel file are ready to use or is it the case that I need to do some other calibration using, for example, a piece of aluminium as described in the YouTube video relating to the unpacking of the device. Is there some document regarding this issue? It would really be good to the get the entire story on calibration/correction of raw data for both Reflectance and Absorbance modes. Any help would be much appreciated.