Other Parts Discussed in Thread: DLPA3000, DLP2010
Hello everyone
I prototyped the board using the following parts.
Controller: DLPC3470
Driver: DLPA3000
The controller farm of DLPC uses the firmware "dlp2010evm-lc_7.3.1.img" of DLP2010 EVM-LC-FW.
However, the board's boot sequence does not work well and [HOST_IRQ] from the DLPC remains high and does not fall low.
[PARKZ] and [RESETZ] from DLPA appear to have been entered successfully.
Is it possible to use "dlp2010evm-lc_7.3.1.img" for the DLPA 3000?