This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need for maximum speed

Other Parts Discussed in Thread: DLPNIRNANOEVM, DLP7000, DLPC410, DLPA200

Hi,

I am new to DLP technology and I have an answer about the maximum speed I can achieve.

I want to use a DLP to build a fast spectrometer in the visible range. To do it I would like to use a grating to divide light in different wavelengths, each one directed to a different column of the DLP mirror array. Then I want to activate only a row at a time at the fastest possible speed. To understand the maximum speed I can achiev with a DLP-based solution I need to know how the digital programming of the DLP works: does the controller sends a command for each mirror pixel using a serial communication? (in this case I think the maximum speed I can achieve to change from one configuration to another is relatively low, since I have to wait that all pixels are addressed). Or is it possible to  control only a couple of rows and leave all other pixel unchanged to maximize speed?

Can you suggest me the fastest solution you have available for my problem?

Thank you for your time,

Best regards,

Alessandro Cominelli