This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR6500EVM: How can I sync the DLP with an external device? I can't find documentation on using the clock (OCLKA connector)

Part Number: DLPLCR6500EVM

I am working with  the 6500 EVM module and would like to sync the patterns changing with an external device. I see the J5 connector with the OCLKA connector for the clock on the EVM. Is there a specific connector I need for the board or specific protocol I should be using to read the clock data to control the other device?

Thank you!