This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC2607: DLPC2607

Part Number: DLPC2607
Other Parts Discussed in Thread: TIDA-01473,

Where is the GUI referenced in the manual for programming/debugging the I2C interface? I can't find it anywhere on the TI web site.

  • Hi Jonathan,

    Welcome to DLP forum and thank you for your interest in DLP technology.

    Could you please share details about the your hardware platform? Is it TI EVM or your own system?  Please provide link to programmers guide you are referring.

    regards,

    Vivek

  • HI Vivek,

    We are using a TI EVM. The programmer's guide is located at:

    http://www.ti.com/lit/ug/dlpu013a/dlpu013a.pdf

    We are using the TIDA-01473 referfence design evm available from TI. The 2607 is the controller for the DMD device. The link to that page is

    http://www.ti.com/tool/tida-01473?jktype=design

    We plan to use it with an HDMI to RGB converter -- that is, without a beaglebone. Regardless, we'll need to access the display settings and the easiest way to get started with that would be to use a gui interacting with I2C via a usb to i2c adapter, as suggested in the programming guide. However, I can find no GUI. Thanks!

  • Hi Jonathan,

    The GUI referenced in the DLPC2607 on programmer's guide is for a discontinued third party party (DLPC2607+DLP3000)  EVM.  I am sorry for confusion it has caused ,we will update programmer's guide.

    Is HDMI to RBG board is an exiting /off-self board? If you are designing that board, you may want to consider adding a micro-controller. In case you want to control from a PC then you will need a USB to I2C board.  

    regards,

    Vivek