Hi,
I need to display patterns at custom bit-depth while receiving 60Hz 24-bit external video feed.
I have previously used the DLP Pico v2 (5+yrs ago) which allowed the 1440Hz binary pattern mode to be setup trivially.
However, having downloaded different EVM GUIs, I am not able to figure out how to enter the 1440Hz binary pattern mode with the DLPDLCR3010EVM-G2.
What I need is the Lightcrafter to take the 60Hz 24bit input and display it as 1440Hz 1-bit monochrome output
Is this even possible with DLPDLCR3010EVM-G2 or have I bought the wrong EVM?
Thanks.
Abe