This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR4710EVM-G2: Abnormal flashing when using DPP3439 V7.3.2 img file to drive LED & NEW DMD(DLP4710AFQL)

Part Number: DLPDLCR4710EVM-G2

Hi

  Attached image file shows a abnormal flashing of LED when power on the EVM Board to switch the splash pattern. This flashing 

doesn't happen on test pattern switch, and the original FW we used that generate from V7.3.2 project files shown as below. 

Please help us to solve this LED problem.

thanks

Device:

DLPDLCR4710EVM Board

NEW Process DMD(DLP4710AFQL)

SW Tool:

Light Crafter Display V7.0-4710EVM

TIRef_DPP3439_p47-1080P-TRP_v7p3p2-PAD3005-AC-Only-TI-com

  • rongyu tu said:

    Part Number: DLPDLCR4710EVM-G2

    Hi

      Attached image file shows a abnormal flashing of LED when power on the EVM Board to switch splash patterns. This flashing 

    doesn't happen on test pattern switched, and the original FW we used is generated from V7.3.2 project files as fllows. 

    Please help us to solve this LED problem.

    thanks

    Device:

    DLPDLCR4710EVM Board

    NEW Process DMD(DLP4710AFQL)

    SW Tool:

    Light Crafter Display V7.0-4710EVM

    TIRef_DPP3439_p47-1080P-TRP_v7p3p2-PAD3005-AC-Only-TI-com Click here to play this video

  • Hi Rongyu, 

    Welcome to TI E2E Forums! Can you reproduce the same behavior with the prebuilt FW v7.3.2 which is available on TI.com?

    Thanks & Regards,

    Hirak.

  • Hi Rongyu,

     i have some follow up questions to understand :

    • From where did you get the project file, are you talking about the firmware because on ti.com only firmware is available not project file ?
    • If you have the project, What changes have you made in project to create the firmware ? 
    • you mentioned that you are seeing flashing while power on the EVM board for switching splash patterns not test patterns, What do you mean by power on the EVM for switching splash patterns, Is this a issue related to power on or the switching splash patterns.... What i understood from video, you turned on the projector and splash screen displays on DMD, now if you change it to another splash then you are seeing this flashing but if you change from same splash to test pattern you are not seeing the flickering. Is my understanding correct ? 
    • Have you used the previous firmware version in past, were you faced this flashing in that older version or not ?

    Thanks,

    Navneet

  • We tried, but for our hardware design, the setting of DMD pin mapping option part we need a option 1 setting.

    Thanks

    Rongyu

  • Hi Naveet

    • This project file is provided by TI Field Application Engineer in TAIWAN.
    • here we only change the DMD pin mapping to op 1, add more look indexes, adjust the LED current in batch file .
    • The following videos can explain a flickering when 1.switching splash pattern, 2.no flickering when switching test pattern, 3. switching between test & splash pattern change.
    • Yes, we tried to create a firmware from v7.0.3 file and used to new DMD , but didn't find this flickering problem. 

        Thanks

  • Hi Rongyu,

    Thanks for the detailed explanation.

    can you please do one more experiment, do not change anything except your pin mapping in the release firmware.

    Try one more time with that firmware and let us know if you are seeing the issue. I am not sure this issue is because of adding the more looks or something else. Once you try this experiment, i hope this issue will resolve. But if you want to add the more looks than you need to be careful as we have evaluated the predefined looks for this light engine.

    As you mentioned you haven't seen any issue on v7.0.3, have you changed the looks and mapping option in that firmware as well. 

    Thanks,

    Navneet

  • Hi Navneet

    The pin mapping setting is base on our HW design, therefore i can't do another experiment for this.

    Yes, i had changed looks and mapping option before v7.0.3 firmware release, those change-values between v7.0.3 and v7.3.2 are practically the same.

      V7.0.3 had another issue such as a pattern mark stay on DMD when turn off engine, therefore we need a new project file to support the new process DMD.    

    Thanks

  • Hi Rongyu,

    We are able to reproduce the same here, and we are following up on this issue you are facing. And we will try to fix this in next release.

    We discussed the workaround with our Taiwan FAE's and they will suggest you the workaround for that issue for now. Please contact our FAE for the same.

    Please Let us know, if you face/encounter any other problem. I will be happy to help !!

    Thanks,

    Navneet