This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3000-C300REF: DLP3000 LightCrafter EVM not detected by computer, making noise on powering and not booting completely

Part Number: DLP3000-C300REF

I am presently using a DLP3000 LightCrafter EVM without the Light Engine(removed after buying since I use the mirror array directly with a laser and has been working well for several years) which upon connecting to the power supply makes a high-frequency noise and is not being recognized by computers with the Windows 10, 7 and XP Operating System - even after the correct drivers are installed. As of now, the micromirror array shows the 2 splash screens of the logo and the chipset in different angles, along with the progress bar which stops just before it reaches the ending. The LED next to the DM365 lights up green, as opposed to the flashing red and green. The other LED lights up green as well.


I have tried booting via SD card, however, I presently only have a SanDisk 16GB card available. The button on the driver board(lower board) also seems to be unresponsive most of the time.

Furthermore, I have tried following the procedure mentioned in the FAQ at the following link: https://e2e.ti.com/support/dlp/f/94/t/623283 . However, none of the computers I tried with have been able to recognize the DLP and so as mentioned in Step 4, I don't think incorrect drivers are being installed and I have not been able to get the "USB serial device" under the "Ports" section in the device manager.


Feedback regarding what could be done to fix the above issues would be appreciated. Thanks in advance for the assistance.