Other Parts Discussed in Thread: DLPC900, , DLPC910
Hello,
I need to use the DMD with a large number of images (more than 400) and with a high pattern update rate (greater than 1 KHz). The problem is that both the internal memory and the flash accept a maximum of 400 images and the video mode has a maximum frequency of 60 Hz. I want to know if there is any way to increase the memory to meet the requirements of my application.
Thank you.