This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478: TRIG_IN

Part Number: DLPC3478

Hi,

in DLPC3478 in datasheet there is a following statement regarding 3DR pin:

"3DR.....For light control applications: Reserved for TRIG_IN (Input). Applicable in Internal Pattern Streaming Mode only"

However on "Figure 33 Internal Pattern Streaming Mode" (page 52) GPIO_5 is used as a TRIG_IN. 

Is this just a datasheet issue or is there any meaning behind it?

Thanks

Petr

  • Hi Petr,

    I believe the reference to the GPIO is in error, but I will check to confirm.

    Thanks,

    Kyle

  • Hi Petr,

    As Kyle mentioned "the reference to the GPIO is in error" is correct. 

    So i am repeating the same line as mentioned in Datasheet and you also mentioned in your query 

    "3DR.....For light control applications: Reserved for TRIG_IN (Input). Applicable in Internal Pattern Streaming Mode only"

    We will correct the Figure 33 in our next datasheet update. Thanks for pointing out the issue.

    Thanks,

    Navneet

    Please Click on the Resolve, if you think your issue is rectified.