Part Number: DLPLCR6500EVM
DMD didn't work after using for a period.
Phenomenon:after connecting power line and USB,the D8 and D9 lamps in the board are lighting,and D6 lamp twinkles,the "connected"option GUI is lighting,these phenomenons are same with normal condition.But the downside option stuck in "standby"mode,and can't switch to"normal"mode,and the"Opreating Mode"stuck in"Video Mode",also,we can't control the micromirror turning.
Refering to the e2e,we do some tests,we provide the results In the annex.DLPLCR6500EVM Debug Note(1).docx