This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3433: IBIS model

Part Number: DLPC3433
Other Parts Discussed in Thread: DLPC3430

Hi, Ti teams

Is there has an IBIS model for DLPC3433 ?

Can anyone help me with this matter?

 

Thanks,

Mike

  • Hi Mike, 

    The IBIS model for all DLPC343x controllers can be found on the DLPC3430 tools & software page. I have provided the link below.

    http://www.ti.com/product/DLPC3430/toolssoftware

    Please let us know if you have any additional questions!

    Thanks, 

    Brandon

  • Hi Brandon,

    Which version can I use?

    Because the read me file show some error text. I can't understand the difference between 9 versions.

    Could you help it?

    Thanks 

    Mike

  • Hi Mike, 

    I've included the text from the read me file below. The 9 models are dependent on the VCC_INTF and VCC_FLSH voltages. I can help point you to the correct model if you could share which voltages you will be using, or you can see the below text. 

    Please let us know if you have any questions!

    Thanks,

    Brandon

    "DLPC343X IBIS Model Notes: (Updated 7/25/2018)

    There are 9 possible combinations for the DLPC343X IBIS models depending on how the chip is implemented in overall system design.

    Since the ASIC voltage rail [VCC_INTF] is variable between 1.8v, 2.5v and 3.3 volts and separately the ASIC voltage rail [VCC_FLSH] can be 1.8v, 2.5v and 3.3v, this requires the different associated IBIS models for all 9 configurations. The following IBIS model versions are as follows for the associated Voltage difference options.

    The customer should use the IBIS model that reflects their respective design setup:

                     VCC_INTF                VCC_FLSH
    Version 1:     11_18 IBIS models      11_18 IBIS models
    Version 2:     11_25 IBIS models      11_18 IBIS models
    Version 3:     11_33 IBIS models      11_18 IBIS models
    Version 4:     11_18 IBIS models      11_25 IBIS models
    Version 5:     11_25 IBIS models      11_25 IBIS models
    Version 6:     11_33 IBIS models      11_25 IBIS models
    Version 7:     11_18 IBIS models      11_33 IBIS models
    Version 8:     11_25 IBIS models      11_33 IBIS models
    Version 9:     11_33 IBIS models      11_33 IBIS models"

  • Hi Brandon,

    Thanks for your help.

    Mike