This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010: How to communicate through i2c with the DLP3010 on raspberry pi 3b+?

Part Number: DLP3010
Other Parts Discussed in Thread: DLPC3438, DLPC3433, DLP2000

I'm trying to communicate through i2c with the DLP3010 on raspberry pi 3b+.

I'm also using the i2ctools to send command to the DLP3010.

I can detect the device using i2cdetect -y 3,  i don`t is that right?


What I wanna do is to Write Keystone Correction Control and Write Keystone Projection Pitch Angle.

 

But it doesn't work at all .nothing happen..

Maybe I misunderstood something. Do you have any idea what I'm doing wrong?

Thanks in advanced.