Part Number: DLP470TP
I am looking for an end-product which will have the option to be able to switch between 60,120,144 or 240hz 1080p or 4K@60Hz.
Will the DLPC itself be enough to add this functionality or will the FPGA firmware need to be rewritten as well?
If the latter, is the FPGA code available in sourcecode form or only binary? Binary is useless for modification purposes.