Part Number: DLP2010EVM-LC
Hi,
I see RGB Led Max Current has a maximum possible setting of 1023.
However, the the Firmware for the DLP 2010 EVM LC ships with RGB Led Max Current set to a very conservative 302.
Is the design safe to run at RGB 1023 without further consideration (subject to the principle that higher current reduces LED lifetime) or is there a risk to fast burnout?
Perhaps it is only safe to take one Led that high and then use monochrome?
Are there any guidelines as to what is safe please?
Regards,
Anthony