Other Parts Discussed in Thread: DLP7000,
HI,
I saw in the product's datasheet in section 7.4 that the maximum illumination power is 0.68 mW/cm^2 in the range under 420 nm wavelength.
But in other products like dlp7000 there was a different section that said on the range of 400-420 nm it can be illuminate with power up to 11 W/cm^2.
I wonder why there is such a big difference between the two products and maybe my dlp4500 can be also illuminate in 405 nm with more power then 0.68 mW/cm^2
This would help me a lot because I need the use a blue laser (405 nm) in order to perform my experiment.
Thank you in advance,
Elyasaf