This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dlp 3010 evm lc do not output signal

Other Parts Discussed in Thread: DLP3010

I want to get the  signal from the trigger out2 when the dlp3010 project patterns we set in advanced,the setting of the software is attached.

Its weird that the function generator displayed 3.3v whether we project patterns,in my opinion is that function generator will display 0V if we do not project patterns,

it seems that the signal can not output normally,so that we can trigger our camera to take photos ,is there any other setting we need to do in the software or if our dlp3010 is broken?