Hello.
I tried to put external trigger into my DMD, but failed.
I am using 51021-0600 for connector and 50079-8100 for crimp.
I put a rectangular wave which is 1kHz, and 3.3V, but it didn't work.
So I checked whether trigger out was working well or not.
Checked by the oscilloscope, it also didn't work.
It can be a connector problem? If not, what should I do then?
Thanks.