This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3000-C300REF: DLP3000 is not connecting to GUI

Part Number: DLP3000-C300REF
Other Parts Discussed in Thread: DLP3010EVM-LC

Hello,

I'm currently using a DMD DLP3000 and it is not connecting to the GUI sofware. I've tried many things already. First I tried installing it to a Windows 7 computer, following the instructions from the manual (Installing the GUI, installing the RNDIS packets and fixing the start-up delay) ; however, the software was unable to connect to the DMD.

Later I tried with a Windows 10 computer, I updated the packages for the USB ports and followed the steps to configure the RNDIS port. I downloaded the DLP LightCrafer GUI and changed the IP address as suggested in the manual to fix the USB-startup delay. Still, the GUI is not able to connect to the DMD