Part Number: DLP3000-C300REF
Hello,
I'm currently using a DMD DLP3000 and it is not connecting to the GUI sofware. I've tried many things already. First I tried installing it to a Windows 7 computer, following the instructions from the manual (Installing the GUI, installing the RNDIS packets and fixing the start-up delay) ; however, the software was unable to connect to the DMD.
Later I tried with a Windows 10 computer, I updated the packages for the USB ports and followed the steps to configure the RNDIS port. I downloaded the DLP LightCrafer GUI and changed the IP address as suggested in the manual to fix the USB-startup delay. Still, the GUI is not able to connect to the DMD
In case this information is relevant, the LED closer to the input button is blinking (red and green).
I hope you can help me to solve this prolem.
Best,
Arturo