We have procured 4 NANOEVM, out of which one device is giving trouble in scan or going to bluetooth mode.
Issues:
1. Base of EVM heats (~60 degree C), which is not observed in other 3 EVMs
2. When I try to put it in ble mode, by pressing the ble button for 5 sec, nothing happens, and if that button is pressed again, it shows ble error on UI with blue LED blinking fast.
3. If I trigger scan from UI, it gives an error.
4. I tried to reflash the TIVA firmware from UI, but that is stuck at 10%
I feel there is some hardware issue with this particular EVM. Kindly suggest the steps to verify issue or any ways to rectify the same.