This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: EVM Light turn on and then off

Part Number: DLP4710EVM-LC


Hello Kyle and other friends

I can't find my posted question, so I post it again.

I just bought a 4710EVM from TI.
When I opened it and tested it with splash images, everything is ok.
Then I stored a pattern to evm, it took a long time, the green bar is still progressing for a long time, then I tried to turn off the power.
When I turned it on again, the GUI shows (EVM connected, powered off), when I push the pb switch, the light turn on for a few second and turn off.
The power adapter is 19V, 4.71A, I bought it from Mouser by clicking the link on the TI DLP4701EVM LC web page.
Thanks!
Derlin