Other Parts Discussed in Thread: DLPC3479
Hello TI,
J48, pin 5 is said to have following functions, could you please explain more of its usage?
For light control applications: Reserved for external trigger signal (Input). Applicable to internal pattern streaming mode only.
Question: Can I pull this pin high to start pattern streaming?
The 3DR pin on the DLPC3479 can be used as a 3D left or right reference indicator or as trigger input signal for light control application. Could you please explain it more on the left/right reference indicator?
A jumperonJ8 and J9 has to be set to determine the use case for this pin. For display application: Connect pin 1 and pin 2 of J8 (DLPC3479Master) and pin 1 and pin 2 of J9 (DLPC3479 Slave). For light control application: Connect pin 2 and pin 3 of J8 (DLPC3479M aster) and pin 2 and pin 3 of J9 (DLPC3479 Slave).
Are my EVM jumpers set for let/right indicator or light control?
Thanks!
Derlin