This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR4500EVM: possibly defective issue DLPLCR4500EVM

Part Number: DLPLCR4500EVM

Hi there,

Our Customer bought DLPLCR4500EVM.

But it doesn’t look too good. It’s colors went much more RED or PURPLE than normal DLPLCR4500EVM.

It also even turns on, Startup Logo “DLP LightCrafter 4500” is also turned RED and PURPLE.

 

He knew something wrong with it.

 

Cause he has another Two of these exactly same products. So This is his third(Latest) one. And also he put same program for other two of those as well and Those work perfect.

He tested with same cables, though.

 

So in this case RGB is broken or needs to be recalibrated, isn’t it?

If anyone knows how to fix this issue please let me know.

 

Thanks!