This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2000: Disable BBB video buffer?

Part Number: DLP2000

I'm not entirely sure I'm on the right track. However, I'm working with  Structured_light code. What I'm seeing is this. When I run the software the Linux desktop is intermittently loading up between frames I load onto the DMD. The slower I run the software the more likely the desktop forces its way in. 

Am I off base thinking between the time I unfreeze the buffer and the next time the software freezes the update buffer the desktop has pushed its own frame onto the buffer? Is there a way to disable the desktop output, so that the buffer only loads what I provide it?

I do not need the desktop at all.