This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Incident Angel Wavelength



Hi Team,

My Customer is looking at our (1) DMD working at 400-700nm, does the incident angle wavelength-dependent? and does the incident angle sensitive? (2) can a  DMD reflect a broadband light source say 500nm - 900nm? Any inputs are appreciated.

Regards,

_Renan

  • 1. Can a DMD reflect a broadband light source say 500 nm - 900 nm?

    TI DLP manufactures DMDs with performance optimized for three different optical bands

    High speed visible nominally 400-700 nm
    Near-infrared (NIR) nominally 700-2500 nm
    Ultraviolet (UV) nominally 363 - 420 nm

    Depending on the customers system performance needs, either a visible or NIR DMD may work for 500 nm - 900 nm operation

    See http://www.ti.com/dlp-chip/overview.html

    DLP application note DLPA031 has details regarding the optical performance of each window design

    See http://www.ti.com/lit/an/dlpa031d/dlpa031d.pdf

    2. Incident angle wavelength-dependent?

    Incident angle of the optical source is typically not wavelength dependent. Incident angle is a critical optical design parameter to achieve the best optical performance.