This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMD problems



Hi,

I'm trying fault find a DLP projector (getting very little help from the manufacturer), which runs two DDP 3021 chips to a Darkchip (1910)1920 x 1080 DMD. The right half of the screen shows vertical lines which have been displaced, giving echo images. I initially thought this was a warm up problem, however this is not so. Periodically the fault clears then re appears, kind of a sync drift.

Is this type of problem likely to be the DMD chip, or one of the 3021 chips?.

Looking at the way the 3021 addresses the display I am guessing it is one of the 3021s. 

Anyhelp would be much appreciated.

One other question, are thw Darkchip1 thro darkchip 4 all pinout compatible?

Thanks

Pete