This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC900: USB PID

Part Number: DLPC900

DLPC900 has a USB module. I would like to modify a default PID because 1 PC controls multiple DLPC900s. Can I do It?

Regards,
Uryyy

  • Hello Uryyy,

    A PID is a "Product ID" and cannot be changed by the end user. 

    The device instance is tracked by windows.  The first device enumerated by windows with this VID/PID is device "0" and the next is device "1", etc. . . 

    Currently there is no methodology documented as to how to address more than one attached system.

    Fizix