Dear Kyle,
I could eventually solve it. Thanks for your help.
I have another question, I would like to use the 1-bit monochrome mode of the EVM. For that, I have to use an external input via the HDMI port, right?
I assume that I will need to use an FPGA to send my patterns to the EVM then. Do you have a suggestion of a certain module that I can use to do that? I do not want to do it through an FPGA and I prefer to create my patterns via Matlab because it is easier and faster.
Any suggestion/reccomendation?
Thanks in advance.
Kind regards,
Anas