I am trying to figure the right DMD and controller board for my application. I have two control boards DLPC900 and DLPC910 for the DMD I am interested in in the EVM kit. The problem is I do not know how much on-board RAM (if any) do these boards offer? to explain more the problem, I have some fixed patterns which I want to send to DMD. Apparently if I want to communicate those patterns to the board each time, my fps would drop simply due to the limited connection bandwidth. I think if there is an on-board RAM then I could pre-load these patterns into on-board RAM and then increase the frame rate? what is the frame rate then with or without using this on-board RAM? Thanks and sorry if the question is so obvious.