This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC350: Light Crafter 4500 EVM is no longer connected to GUI

Part Number: DLPC350

Hi,

I have ben using the driver board of Lighctarfter 4500 for over a year and it was working properly until todat when I chnage the firmware option to fast flash update. Then the GUI crashed and since then the lightcrafter is not connected to the GUI. When I discconet the power cable and connect ir again, there id a red light on the other side of the board which lights up just for a sencond.

Sis