This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3470: issue of 1-bit external pattern

Part Number: DLPC3470
Other Parts Discussed in Thread: DLP2010

Dear Sir/Madam:

I meet a issue when I use the DLPC3470 to control dlp2010. Please refer the detailed description below.

Backgroud: DLPC3470;DLP2010; 1-bit  Mono external pattern; 15 1-bit patterns; 

Issue: As the snapshot attached, the other patterns will be impacted by one horizontal stripes pattern.

I have monitored the data signal with oscilloscope, the quality is good. Please help to analyse the issue.

Best Regards