This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Light Commander Modularity



Looking at the schematic, I noticed that many of the parts of LC are modular, and I assumed that we could isolate the working DMD chip from all the optical components.  I just want to make sure that this is the case.

We are seeking to build an optical system around the DMD chip using our own equipment so we need a very clear and unobstructed path to and from the DMD chip for our own system's illumination and collection arms.  Is it possible to remove all the optical components so that we can do this and still control the chip?

If not, would you suggest just buying the chipset (http://focus.ti.com/paramsearch/docs/parametricsearch.tsp?family=analog&familyId=1746&uiTemplateId=MDLP_PARMSRCH_T&paramCriteria=no)?  Am I correct in assuming that the chipset is standalone?  Also, what type of software comes with the chipset that allows control over the DMD?  I could only find the API for the LC, and that software will probably not be included if I buy only the chipset...