This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I recently got a DMD DLP 7000 UV.
Any suggestion regarding how to mount the DMD vertically?
It seems that no holes on the backside are available?
Hello Qiang,
For bench mounting a large lens holder actually works fairly well. You can capture the sides of the PCB in the V channels or the sides of the aluminum "face plate"
It is possible to also carefully disassemble the mounting hardware and tap some holes on the lower edge of the face plate to attach a block that will mate to 1/4-20 mounting post.
Fizix