Part Number: DLP4500-C350REF
We are working with the DLP LC 4500. We want to display the following sequence: an image similar to the "Solid Field" Internal test pattern in video mode, and then turn the display OFF for a specified amount of time, and then display the image again. How can we do this in the pattern sequence control? When we upload a blank image, the DLP does not turn off. It continues to display kight. We would like the DLP to not display anything automatically, similar to pressing "Stop" in the pattern sequence control, without having to manually press stop.