Other Parts Discussed in Thread: DLP2010NIR, TIDA-00554
Dear DLP support team,
I have checked the DMD used in DLPNIRNANOEVM and DLPNIRNANOEVM datasheet and saw that although the DMD has optimized wavelength between 700-2500nm, the EVM has optimized wavelength between 900-1700nm.
Can I ask the reason behind this issue?
I am working on a project where I have to analyze the spectral response of a chemical between around 700-2500nm. I also think that the InGaAs detector used in EVM can also operate upto sth near 1650nm.
Do you have any recommendation on how to modify the optoelectronic part to change the wavelength range of EVM to 700-2500nm? Is it possible?
I found TI DLP EVM that can operate between 1350-2450 nm, but I am planning to target 700-2500nm range using single device.
Thank you very much for your help in advance.