Part Number: DLPLCR6500EVM
Hello,
I am trying to get acquainted with this equipment and I started by following the quick guide present in the manual of the DLP.
First of all, I started by powering up the device: all the LEDs are blinking in the right way and, as soon as I power up the device, I can see some extra diffracted orders (which means that the something happens when I connect it to the power); differently to what reported to the manual, I can't see a continuous pattern after 5 seconds (this is the first difference with respect to the guide).
Secondly, I connect the device to the PC through the USB cable and I open the DLP LCR6500 _ LCR9000 GUI 4.0.1. I can see from the System Control that the chip is connected, but it goes to by default to Chipset Type DLP9000 (I don't know if it is normal, in any case I switch to the DLP6500, the right one). At this point I start creating the first sequence, like in the manual, through the Pattern On-The-Fly Mode. The first issue I have is that, after selecting this modality, the selection goes automatically back to Pre-Stored Pattern Mode. I saw that the only way for which the selection stays in the Pattern On-The-Fly Mode is when I select Standby.
At this point I am not able anymore to follow the example present in the Quick Start section of the manual, since the operation mode is different. However, I tried also to use the Pre-Stored Pattern Mode by following one of the tutorials I found on the TI website but there was no way to see any change in the pattern.
The setup I used was built in this way: a green laser source impinging on the DLP, whose reflected light is projected onto a wall. Of course, I did see all the diffracted orders but I couldn't find any movement of the pattern (except a small variation when I powered up the device). The connections from and to the device were simply the power connection and the USB one.
At this point, I don't know if the problem is on the device or on the software, which doesn't communicate with the DLP.
Thank you in advance for your help.
Best regards,
Matteo