Hello,
I am trying to connect DLP NIRScan EVM to a Windows 10 PC. It appears that the EVM is not able to communicate with the PC. I have tried two different approaches:
1) Used the http://192.168.0.10 IP address to try to connect to the EVM over the USB cable but the site is not found and the request times out repeatedly.
2) Downloaded the GUI which does get properly installed but does not show 'Connected' at the top. Tried multiple times with various combinations of starting the GUI and connecting the cable but to no avail.
I suspect the problem lies in a device driver not being present. It could be the RNDIS driver. When the EVM is connected to the PC then it simply enumerates as a USB device not as a COM port or an ethernet port. I am not sure how to install the RNDIS driver which I have downloaded but comes as a .cat file. Any help will be greatly appreciated.
Thank you,
Faiz Rahman
Ohio University
Electrical Engineering