If I use NIR(1550nm) source with Light Commander, I will loose around 20% of it from front window of DMD for only one transmission through the window, see http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/94/t/85503.aspx, which is reflected from front window. Can anybody explain that where does this reflected light from the frond window of DMD go? it goes back to the source or some other directions. Can you a little bit elaborate this reflected light from front window in terms of directions it goes?
Second question is that if I buy only DMD and Controller Board of Light Commander (they are available separately from Light commander) do I need any extra hardware and software set up to be able to pattern mirrors? Can I use software developed for LC if I only buy DMD and Controller Board?
Thank you