Hi Im looking for a recommendations on a true 4k DLP chip for single wavelength (UV/NearUV 405nm) for the use on a resin curing printer Im working on. Its a personal project so i wont be looking to mass produce.
But i would like some recommendations on 4kDLP chips, ideally 8bit+ greyscale, an evaluation controller board would be useful as well.
And of course affordable.... As this is not a full entertainment projector project. I dont need super high mirror response times for RGB filtering. Just fast enough to give me 8 to 12 bit greyscale for a single wavelength.
This is also assuming that UV wavelengths dont damage the DLP chip.
So any recommendations?