Hi,
I'm testing a DLP2010EVM-LC model using DPL Pico Display and Light Control EVM GUI (Advanced), and want to write internal pattern data(.bin) to firmware's flash area.
I have followed instructions on Chapter 3.7 Flash Update Commands on document dlpu075a, but when I tried to do Write Flash Start, it occurs some error and the firmware uploaded at the projector seems to be crashed after that. (It works well after whole firmware is uploaded again)
Actually, I have no idea which form of data(.bin) is right to input to the text box below.
I have tried hex and ASCII code, but it occurs error again.
What can I do for the Write Flash Start operation on the GUI?
Regards,
Son