This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR2000EVM: Turn DMDs ON and OFF with the LED light on

Part Number: DLPDLCR2000EVM
Other Parts Discussed in Thread: DLP2010, DLPC3430, DLP2000, DLPC2607

Is there a function that allows turning the DMDs ON and OFF while keeping the LEDs ON? DPP2607_Write_DmdPark() seems to control both the DMD state and the LED state simultaneously (because absolutely no light comes out of the opic engine, unlike DLP2010).

Thanks!